BEGIN:VCALENDAR
VERSION:2.0
PRODID:-//www.twentythree.net, see addthisevent.com for calendar stuff though//EN
BEGIN:VEVENT
DTSTAMP:20260728T154500Z
STATUS:CONFIRMED
DTSTART:20260728T150000Z
DTEND:20260728T154500Z
SUMMARY:Closing the intralogistics loop with mobile cobots (US)
DESCRIPTION:https://video.universal-robots.com/closing-the-intralogistics-loop-1 \n\n***Most cycle time isn't work. It's parts waiting to move.*\n\nMost plants never measure it, but it’s there in every shift. An \noperator leaves the station to fetch material. A machine sits idle \nwaiting on tending. A work cell stalls because the last part hasn’t \nshown up yet. It isn’t a labor problem or a machine problem. It’s a \nmovement problem and it stays invisible until you add up the minutes.\n\nThis live webinar looks at mobile cobots: machines that don’t just \ncarry parts between processes, but pick them up, handle them, and put \nthem to work the moment they arrive.\n\n****What you’ll learn*\n\n-\n\nThree real deployments, live: Transport, machine tending, and \npick-and-place, running in actual production environments\n\n-\n\nWhy “fixed infrastructure” is the wrong question: How these systems \ndeploy inside the layout you already have, no rebuild required\n\n-\n\nThe ROI math, explained: A model you can apply to your own floor and \nscale use case by use case\n\n-\n\nWhat happens after use case #1: How an open ecosystem turns a single \ndeployment into a growing capability, instead of a one-off project\n\nIf material flow is the quiet bottleneck nobody’s tracking, this is 45 \nminutes worth blocking off to attend.
X-ALT-DESC;FMTTYPE=text/html:<!doctype html><html><body><p><a href='https://video.universal-robots.com/closing-the-intralogistics-loop-1'>Closing the intralogistics loop with mobile cobots (US)</a></p><p><h2><strong>Most cycle time isn't work. It's parts waiting to move.</strong></h2><p>Most plants never measure it, but it’s there in every shift. An operator leaves the station to fetch material. A machine sits idle waiting on tending. A work cell stalls because the last part hasn’t shown up yet. It isn’t a labor problem or a machine problem. It’s a movement problem and it stays invisible until you add up the minutes.</p><p>This live webinar looks at mobile cobots: machines that don’t just carry parts between processes, but pick them up, handle them, and put them to work the moment they arrive.</p><h3><strong>What you’ll learn</strong></h3><ul><li><p>Three real deployments, live: Transport, machine tending, and pick-and-place, running in actual production environments</p></li><li><p>Why “fixed infrastructure” is the wrong question: How these systems deploy inside the layout you already have, no rebuild required</p></li><li><p>The ROI math, explained: A model you can apply to your own floor and scale use case by use case</p></li><li><p>What happens after use case #1: How an open ecosystem turns a single deployment into a growing capability, instead of a one-off project</p></li></ul><p>If material flow is the quiet bottleneck nobody’s tracking, this is 45 minutes worth blocking off to attend.</p></p></body></html>
BEGIN:VALARM
ACTION:DISPLAY
TRIGGER:-PT15M
DESCRIPTION:Closing the intralogistics loop with mobile cobots (US)
END:VALARM
END:VEVENT
END:VCALENDAR