Base Connector - Cobots on the move

Universal Robots+

|

 00:41

The GRIP Base Connector allows quick and easy removal of the entire robot arm. The Robot arm is bolted to a quick Connect system which in turn is bolted to a table or cell. This manual Connect system allows companies to use the same robot in multiple different cells without having to unscrew the robot every time. A simple lever allows the robot to be released from its current position and taken to a new position. The entire process takes only a few seconds. It enables companies to be more flexible with the robots that they have and optimizes the use of their resources.