[Case Story] SEAO_SG_Seng Heng Engineering EN
Seng Heng Engineering, a third-generation manufacturer with 70 years of experience, is a single-source solution provider of fasteners, turnkey machining and corrosion resistant coating products. Due to rising manpower shortages, Seng Heng Engineering has installed two UR10e collaborative robots (cobots) from Universal Robots in the production line to automate the CNC and engraving processes. The manufacturer has witnessed a significant increase in productivity and efficiency after the deployment of UR cobots. Now, the cobots are working round the clock in tandem with human workers, relieving humans from tasks previously performed manually while increasing work efficiency.