Case Studies

Case Study Video YUEYIN TECHNOLOGY UR5 Pick and Place .mp4

YUEYIN Technology’s Memory Module Production Line is equipped with 4 UR5 Robots. UR Robots' features of flexible deployment and fast set-up enable YUEYIN Technology to arrange equipment on production line and adjust processes, which accelerate the innovation of work flow to deliver high-quality customized products. In addition, for each UR5 Robot that YUEYIN purchased, the cost can be covered on an average period of 8-9 months, which is beneficial to the company’s fund allocation and also provides more flexibility to the operations.