Robot Base Station
Utilize the robot at several workstations. The Robot Base Set makes it easy to move the robot to another workstation without unscrew the robot every time. Fasten the robot to the Master Plate and fasten the Base Plate to the other workstation and the robot is ready to perform. For example, let the robot perform a welding task at first workstation and move it to the assembly line the next few hours. The patented design of the Robot Base secures exact zero-positioning every time so no need for reprogramming.