TracePen
With the TracePen it is possible to teach a robot in a matter of seconds by simply showing it the path to be learned by moving the TracePen. This movement is visualized almost simultaneously in the app by the Wandelbots software and can be further refined by defining individual points (keyframes). The keyframes can be adjusted in the sub-millimeter range via the app. Define whether the robot should move from point-to-point, linear or circular between the defined points. The built-in joint control allows the user to directly control the individual robot joints and even define a safety area by allowing the robot to act. Teaching complex motion has never been so easy!