UR3 - the worlds first table top cobot
About Universal Robots
|
02:27
UR3 is our new, smaller collaborative table-top robot for light assembly tasks and automated workbench scenarios. The compact table-top robot weighs only 24.3 lbs (11 kg), but has a payload of 6.6 lbs (3 kg), 360-degree rotation on all wrist joints and infinite rotation on the end joint. These unique features make UR3 the most flexible, lightweight, collaborative table-top robot to work side-by-side with employees in the market today. It’s an ideal choice for applications that require 6-axis capabilities where size, safety and costs are critical.