Welding Package - Trace Pen
This system makes programming a lot easier. Due to the simple operation, which is intuitive, component programming can be done with very little training. In addition, the programming time for an assembly is greatly reduced, so that small batch sizes can now also be automated economically. The system even allows the components to be programmed outside of the robot system - this increases system availability. The data is sent to the robot (from different manufacturers - standardized) and accepted.