About Universal Robots

Cobot presentation

May 18, 2016 cobot presentation, demo, ur5
The founder of Universal Robots, Esben Østergaard demonstrates the lightweight collaborative and flexible Robot UR5 which lets you automate repetitive and dangerous tasks with payloads of up to 5 kg. UR5 is a Low-weight collaborative robot that can be used for tasks such as: picking, placing and testing, machine tending and many other tasks. With a working radius of up to 850mm, the UR5 collaborative robot puts everything within reach, freeing up your employees’ time to add value to other stages of the production.
The UR5 fromUniversal Robots is very easy to program, offers fast set up, is collaborative and safe, and like our other collaborative robots, offers one of the fastest payback times in the industry. You can read more about the advantages of a collaborative robot from Universal Robots here www.universal-robots.com/products/ur-robot-benefits